Permanently locked out from ADuC7024 after entering Nap Mode.

I've been testing switching from internal oscillator to external crystal using the procedure in the device data sheet (Rev C, page 55) and reproduced below. (This procedure was not in Rev A datasheet). This code is placed just after entering main() of the application

T2LD = 5;
TCON = 0x480;
while ((T2VAL == t2val_old) || (T2VAL > 3)) //ensures timer value loaded
IRQEN = 0x10; //enable T2 interrupt (commented out this line)
PLLKEY1 = 0xAA;
PLLCON = 0x01;
PLLKEY2 = 0x55;
POWKEY1 = 0x01;
POWCON = 0x27; // Set Core into Nap mode
POWKEY2 = 0xF4;

I commented out the IRQEN line (to try something out) and built and ran the application. Since this time I have not been able to access the ADuC to re-program it. I am using IAR EWARM and a miDAS J-Link. I get error dialogue messages along the lines of "Unable to halt the ARM core".

I have tried holding the !RST pin low while powering up and then accessing using JTAG and other conditions, but I seem to be permanently locked out of the device. By holding !RST low while powering up I expected the ADuC7024 would not execute (the above) code to enter nap mode and that I could then use the JTAG connection to reprogram with a program that does enable the wakeup timer IRQ.

There is a related thread http://ez.analog.com/thread/3969 ("When debugging the ADuC70xx parts via JTAG, I sometimes encounter problems where the JTAG interface no longer works?"). I am not able to use ARMWSD to try a mass erase as the application has SIN and SOUT mapped to pins other than P1.0 and P1.1 and those pins have other uses.

Is there any way to recover? Also, why am I locked out, as I mentioned earlier I expect that if I hold the device in reset on power up it would not enter nap mode?

I could do with changing the bootloaded/kernel to map the UART to pins other than P1.0 & P1.1, but accoring to http://ez.analog.com/thread/3984?tstart=30 this is not possible.

Parents
  • As a general rule for all developers I would suggest that they place a 1 second delay at the start of their code at least during the development phase.  This then allows them to gain JTAG access to the part before any problem code gets executed.  If such delay is unacceptable a spare pin could be used that will put the part in a loop to allow JTAG to gain access without reaching the offending code.  As long as you can gain JTAG (debug) access you can erase the code and put on corrected code.  These tricks can be removed for the final product after development is complete.

Reply
  • As a general rule for all developers I would suggest that they place a 1 second delay at the start of their code at least during the development phase.  This then allows them to gain JTAG access to the part before any problem code gets executed.  If such delay is unacceptable a spare pin could be used that will put the part in a loop to allow JTAG to gain access without reaching the offending code.  As long as you can gain JTAG (debug) access you can erase the code and put on corrected code.  These tricks can be removed for the final product after development is complete.

Children
No Data