ADuC7024 ADC - Misc questions

Hi,


I have a few questions regarding the behaviour of the ADC peripheral on the ADuC7024 that I hope can be commented on:


i) After an ADC conversion has completed (ADCReady = 1) are the contents of bits 0 to 15 in ADCDAT all 0 or other/undefined?


ii) Data sheet Rev C, P44 says that reading ADCDAT clears ADCReady (ADCSTA, Bit 0). Does this also clear the ADC Channel (bit 7) in IRQSIG?


iii) With ADCCON configured for conversion on Timer 1 (bits 2:0 = 001) is it acceptable to read ADCDAT after a previous conversion has been performed (ADCReady = 0) and while a new conversion is in progress (ADCBUSY = 1)? I want to avoid the possibility of reading a value that is neither the result of the previous, or current conversion, such as when the result is being transferred internally to ADCDAT?


iv) What happens if ADCCON is written to/changed, while an ADC conversion is in progress (ADCBusy = 1) - does it affect the conversion in progress?


v) What happens if ADC channel is changed (ADCCP) while an ADC conversion is in progress (ADCBusy = 1) - does it affect the conversion in progress?


Thanks.

Parents
  • 0
    •  Analog Employees 
    on Mar 4, 2011 5:32 PM

    (i) Take the value of bits 15-0 as undefined. there content is meaningless.

    (ii) IRQSIG will be cleared by this operation. IRQSIG is used as the input to IRQSTA - once an interrupt source is triggered, it is latched into IRQSTA and the relevant bit in IRQSTA will not get cleared until the interrupt is fully serviced. If you want to determine if an ADC or any other interrupt needs to be serviced then read the IRQSTA register and not IRQSIG.

    (iii) Yes, it is acceptable to read ADCDAT in this way - you just need to make sure that the previous conversion is complete.

    (iv) Writing to ADCCON when a conversion is under way will cause the current conversion to stop and a new conversion to start.

    (v) Same as (iv)

Reply
  • 0
    •  Analog Employees 
    on Mar 4, 2011 5:32 PM

    (i) Take the value of bits 15-0 as undefined. there content is meaningless.

    (ii) IRQSIG will be cleared by this operation. IRQSIG is used as the input to IRQSTA - once an interrupt source is triggered, it is latched into IRQSTA and the relevant bit in IRQSTA will not get cleared until the interrupt is fully serviced. If you want to determine if an ADC or any other interrupt needs to be serviced then read the IRQSTA register and not IRQSIG.

    (iii) Yes, it is acceptable to read ADCDAT in this way - you just need to make sure that the previous conversion is complete.

    (iv) Writing to ADCCON when a conversion is under way will cause the current conversion to stop and a new conversion to start.

    (v) Same as (iv)

Children
No Data