hardware question: is it possible to flash a memory without a debugger ? if so how?

Hello.

I have an ADuC7023. Is it possible to download the program to the uC not "through" debugger ??

I checked the compatibility of ULINK 2 from KEIL, and as can be seen below ADuC7023 is not on that list. That is why I was wondering if it's possible not to have it.

Analog Devices(ARM7/ARM9/Cortex Family)
ADuC7019, ADuC7020, ADuC7021, ADuC7022, ADuC7024, ADuC7025, ADuC7026, ADuC7027, ADuC7028, ADuC7030, ADuC7032, ADuC7033, ADuC7034, ADuC7036, ADuC7037, ADuC7038, ADuC7039, ADuC7060, ADuC7061, ADuC7062, ADuC7128, ADuC7129, ADuC7229

I attateched what I've found in the Internet and I'm not sure if I can connect eg. LPT directly to the uC ??

Help would be appriciated.

attachments.zip