ADUC7026 evaluation board

I am using ADUC7026 evaluation board for my testing. Keil uVision 3 which was supplied with kit i am using for build &load. I am using array of 580 (each of 1 byte) data and working fine. When i add one more array of 580 (1 byte each) values , i am able to build and load in to evaluation board. But it is not working. When i remove one array then its start working. my total program is less tha 2K bytes(when both arrays are present). why it is not working please help me  I would like to know

  • 0
    •  Analog Employees 
    on Feb 19, 2015 9:17 AM

    As indicated on the Analog Microcontroller front-page of this community:

    If you experience problems with running your software project on Analog Microcontrollers,

    please provide a minimal, but complete project, executable on an evaluation-board as

    ZIP-file attachment to your discussion/question.

    This enables us to provide faster feedback for you and to improve your experience with ADuC products

    Complete i.e. means that also in the ZIP-file provided you have included as well all used header files.

    The project should be for actual versions of the Keil, IAR or eclipse/GNU-based tool-chains.

    BTW - you may first of all update the µVision to the actual Version from the Keil WebSite.

  • 0
    •  Analog Employees 
    on Mar 5, 2015 10:03 AM

    Have you done further checks with a updated tool chain?