Hello,
i tried the e.g from this thread
https://ez.analog.com/message/57733#57733
but i cannot get it work. It did not spring into any Interrupt handler.
I have two warnings with cstartup.s file Warning[403]: Deprecated form of PSR field specifier used (use _cxsf)
It is at line 258 and line 325 in cstartup.s
I use IAR ARM and Aduc7061 Evaboard with mIDAS-Link.
Best Regard
Ngoc
i got the solution. The processor mode for VIC must be Arm.
I had the thumb mode before, that's why it did not work.
But the warning is fine, isn't it?