Post Go back to editing

ADuC7020 ~RST (external pin 19) power up behavior

According to the ADuC7020 datasheet on reset P0.6 (pin 19) function is MRST and kernel changes P0.6 default configuration to GPIO. Should I see about 128 ms delay between IOVdd and MRST rising edges during power up? According to my oscilloscope the delay is only 100us. Am I missing something in the datasheet regarding power - on reset operation? 

Parents Reply Children
No Data