Hi,I look for a PC application/tool to program ADuC7026 micro controller's flash on factory path,using JTAG.I use uVision 4 to compile/debug/flash program for ADuC7026. But for factory path is not so good application for ADuC7026 flash program.
So I look for small simple PC application to only program flash of ADuC7026, without any other functionalities. Such application should load a HEX file through USB-JTAG adapter to the flash memory of ADuC7026.
Thank in Advance
Yakov
Hi,
You can use the ARMWSD - ADUC7XXX in-circuit serial programming tool if you have a UART Part or I2CWSD.exe if you have an I2C part to download hex file to the part.
https://www.analog.com/en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/eval-aduc7026.html#eb-relatedsoftware
regards,
Mark