Search FAQs on the left to see if your question has been answered. Click on the dropdown to view all of the documents associated with the product. If you can't find your question, click on Ask a Question.

ADuC814: Digital I/O configuration

Can I program Port 1 and 3 as input or output, ie is it to send logic 1 or
logic 0 via port 1 and 3? In the document, it says, whenever you write 0, it
becomes input. It also says P1.2-P1.7 cannot be configured as digital output.
But it should drive base of a transistor connected to P1.2-P1.7 if I write 1 to
P1.2-P1.7.

 

Each of the pins of Port 3 can be an input or an output. If you write a 0 to
the bit location in the P3 register, the pin outputs a digital low. If you
write a 1 to the bit location, the pin is pulled high by an internal pull-up
and in addition, a strong pull up is active briefly, to speed up the 0-1
transition.

Pins P1.0 and P1.1 fucntion like the port 3 pins. All the other port 1 pins can
only be digital inputs or analog inputs (to the ADC). To get them to be digital
inputs, you need to write a 0 to the bit location in the P1 register. To get
them to be ADC input pins, write a 1 to the port bit and configure ADCCON2.3~0
to select the required channel.

There is no output circuitry on P1.2~P1.7 so thay CANNOT even be used to drive
transistor bases, as you describe.
Comments
Anonymous
Related