Search FAQs on the left to see if your question has been answered. Click on the dropdown to view all of the documents associated with the product. If you can't find your question, click on Ask a Question.

Does ADuC831 have an internal pull-down resistor connected to RESET pin?

1) Does ADuC831 have an internal pull-down resistor connected to RESET pin? If
so what value (in kohms) is it. If no - should I use an external resistor?

2) Is Aduc 831 reset after power-on? Or do I have to use RC on RST pin to force
high state on RST pin to correctly reset the ADuC after power-on.

 

1) There is a weak internal pullup (about 10 kOhm nominal) : if you are worried
about glitches in a noisy environment we suggest you add a strong external
pullup- 1 Kohm should be fine.

2) Power on Reset is automatic.
Comments
Anonymous
Related