Search FAQs on the left to see if your question has been answered. Click on the dropdown to view all of the documents associated with the product. If you can't find your question, click on Ask a Question.

ADUC831:  What is the value of internal pull-ups in ports P2 and P3?

What is the value of internal pull-ups in ports P2 and P3?

 

There are weak pullups on P2 / P3 ports.
You can see this when you look at the datasheet specifications.
Look under "DIGITAL OUTPUTS"
Isource for Voh (page 5) is only 20uAmps / 4 volts.
At higher currents, Voh will fall.
This means that, in most cases, you will have to add an external buffer.
Comments
Anonymous
Related