Search FAQs on the left to see if your question has been answered. Click on the dropdown to view all of the documents associated with the product. If you can't find your question, click on Ask a Question.

ADUC832: How can I check if a single ADC conversion was finished?

I'm using an ADuC832 to monitor/control the unit. To perform the monitoring I
use the internal 12 bit ADC converters. How can I check if a single ADC
conversion was finished.

 

A single ADC conversion is finished when Busy bit in the ADCCON3 register (ADC
Control SFR 3)is cleared by the core. It is set during a valid ADC conversion.
Comments
Anonymous
Related