Search FAQs on the left to see if your question has been answered. Click on the dropdown to view all of the documents associated with the product. If you can't find your question, click on Ask a Question.

What is the maximum Source current, that port P2.5 and P2.6 can deliver?

What is the maximum Source current, that port P2.5 and P2.6 can deliver?  (Note
sink current is defined in datasheet but not source current)!

 

The ADuC847 digital outputs can source up to 80uA and still be guaranteed to
output a valid logic output level (>2.4V).

Comments
Anonymous
Related