Search FAQs on the left to see if your question has been answered. Click on the dropdown to view all of the documents associated with the product. If you can't find your question, click on Ask a Question.

ADUC848: Is there a single device with supply range 2.7 to 5.5 V?

Do you have an ADuC848 working at supply range 2.7 to 5.5 V?

 

It is not possible to get a single  ADuC848 that runs off power supplies of  3-
5 volts. You have to order either the 3V or 5V version of the device (different
silicon). Order an ADUC848 with -5 or a -3 suffix as appropriate.

Comments
Anonymous
Related