Post Go back to editing

Setting UART speed for ADI monitor in Keil uVision3

The settings of ADI monitor in Keil uVision3 seem to only allow to select the COM port, but not the COM port speed.  I tried to change the XTAL speed field in the ADI monitor settings and I tried to change the COM port speed in the Windows device manager, but both without effect on the ADI monitor UART speed. 

Is the communication speed of ADI monitor in Keil uVision3 set in stone to 9600 or is there a way to change that ?