ADUC834 Flash/EE program memory security

Dear 

Please give a hand, for ADUC834,I will use the Secure Mode of ADUC834 of flash/EE,but there are two problems need to be solved,thanks.

1.how to make sure the encryption is successful.

2. when I download the program to Flash, the system promote the large program.

3.is there a good debug tools for ADUC834. 

Parents
  • +1
    •  Analog Employees 
    on Jun 19, 2019 6:52 AM

    Hi,

    This mode only prevents Reading/Verifying the memory in Parallel Mode. Reading the internal memory via a MOVC command from external memory is also disabled. You can try to issue read or verify command (which should fail) to check if this mode is activated.

    regards,

    Mark

Reply
  • +1
    •  Analog Employees 
    on Jun 19, 2019 6:52 AM

    Hi,

    This mode only prevents Reading/Verifying the memory in Parallel Mode. Reading the internal memory via a MOVC command from external memory is also disabled. You can try to issue read or verify command (which should fail) to check if this mode is activated.

    regards,

    Mark

Children
No Data