ADuC847 communication issue

We have been using the ADuC847 for several years. Lately we are getting communication error when trying to reset the controller. The response from the controller indicates its a baud rate error. We tried to replace the crystal or controller and that sometimes work and most of the times do not. We are getting about 10% failures on the production line. We would like to get to the root cause for this problem and would appreciate any help to solve this problem. We are using the ADuC847 52-pin package. In addition some controller would work initially at the manufactures and then later would start getting the same bad characters indicating communication error and does not allow to load any programs.

Thanks

Parents
  • 0
    •  Analog Employees 
    on Jan 24, 2019 7:32 AM over 1 year ago

    Hi,

    You mentioned that you have been using the ADuC847 ago, is it failing on a new application? New circuit design? or is there any changes to the user code?

    regards,

    Mark

  • Hi Mark,

    It is the same design and the problem is directly related to communication and downloading code. When resetting the board rather than obtaining response back indicating the controller version as ADuC 847 or so I get back bad characters indicating communication errors. In production say we manufacture 200 boards, out of the 200 we would get 30 boards with this problem or failure. User code has nothing to do with it and its not a new application or new circuit design. Could this be related to manufacturing issue or maybe moister affecting the controller or the crystal?  

    Thanks

Reply
  • Hi Mark,

    It is the same design and the problem is directly related to communication and downloading code. When resetting the board rather than obtaining response back indicating the controller version as ADuC 847 or so I get back bad characters indicating communication errors. In production say we manufacture 200 boards, out of the 200 we would get 30 boards with this problem or failure. User code has nothing to do with it and its not a new application or new circuit design. Could this be related to manufacturing issue or maybe moister affecting the controller or the crystal?  

    Thanks

Children