Can we read flash contents from ADuC84x by a method except the parallel mode?

We can readback the flash contents by the parallel mode if the flash is not in secure mode or serial safe mode, I understand.

But when using the parallel mode, we may need to remove the device from the board or modifiy the board.

Except the parallel mode, are there any methods to readback the flash?

Are there any ways to readback the flash by the USB-EA Emulator, on the Keil or WSD?



The typo is modified.
[edited by: Euglena at 11:42 AM (GMT -4) on 11 Sep 2018]

Top Replies