Yes.
The threshold current is 75 to 850uA.
Please see datasheet paragraph:
Antenna Switch Control
The MAX2674/MAX2676 ANT input includes an autodetection feature. When no current is drawn from ANT, the switch defaults to normal LNA operation. The pin can be directly connected to an external active antenna. The device automatically switches to the ANT input when an external active antenna is connected.