Question
In the ADL5545 S-parameters provided in the datasheet, gain S12 magnitude is different from the table.It appears, for example, about 20dB on the table in the GHz range, but onlyabout 10+dB on S parameters. As you can see at 2600MHz: table shows 20.9dB andS21 is only 11.59. Maybe there's an error in S21 scale?
Answer
The data file format for s2p is different. It is not in dB. If you remove the dB from the magnitude column , then you can get the correct data.Attached is the one that is converted to the way they are used to, and the most common format.
Please see attached correct data.
Feedback: Modified data received from BU, Kagan Kaya