Question
What applications is this part aimed at?
Answer
The ADA4622-2 can be used in many different applications but it’s very low bias current mean it is particularly suited to interfacing with highoutput impedance sensor interfaces or photodiode sensor interfaces or any application which requires a transimpedance amplifier. The low bias currentalso means that the part is suitable for use in precision filters and signal conditioning and the strong drive strength and the ability to drive a500 pF load directly means that the ADDA4622-2 is also suitable for use as an ADC driver.