Question
Can you clarify if the package for HMC3587LP3 should have the markings 3587 or
H3587? There is confusing information on page 5 of datasheet where in outline
drawing it shows:
While on same page it states marking should be H3587:
Answer
I can confirm that the "3587" marking as in the outline drawing is the correct
marking on the HMC3587LP3 package. The package information section of the
datasheet shows "H3587". This is incorrect and the datasheet will be updated to
correct this to "3587" as soon as is practical.