The MAX3658 is a high-gain amplifier. When the input is floating, and very small disturbance or noise couping at the input can be reflected in the output signal. Even if the input is short-circuited, there will still be an offset voltage of around 2mV.