No. This issue has been investigated by the MAX1452 business unit and it has been determined that Maxim cannot offer this device in higher than +125°C temperature range as neither the package nor the process can be guaranteed in that range.
There is, specifically, no possibility of customizing the MAX1452 for temperature operation outside the existing -40°C to +125°C Automotive temp range.