Can I add ESD protection to the ANT pin in the MAX2674?
Depending on the type of antenna that will be used and the application, ESD protection is recommended. If you plan to add ESD protection, we recommend to look for a suitable part that has the following qualities:
Does not significantly reduce the sensitivity of the LNA.
Does not significantly introduce capacitance for the frequency of operation.