Q
We are using the Part, AD215BY for one of our applications.We got the MTBF of this device is 922,107.40 at 25˚C,But We need the MTBF of
this above 70˚C.
A
We do not have any MTBF data specifically for the AD215, but we do have MTBFdata for the AD210, which is part of the AD2XX family.
These are not monolithic devices. They are surface mount / pc board product
assembly process (passive components, multiple die, etc.), so they don’t fall
under a specific Fabrication Process.
Burn In, reliability monitor data, Early Life Failure, etc. are not available
for this type of process.
Product MTBF
AD210 900 thousand hours