The MAX1452 Evaluation kit software does not allow writing to the oscillator bits in the Configuration register. How can I write to these bits?
The only way to write to these bits with the MAX1452 EV kit software is to generate a flash file with the oscillator bits set to the desired value. Then, using the EV kit software, perform the "Load Flash from File" operation to write the file into flash.