Post Go back to editing

Choose a variable gain amplifier for hall effect sensor output

I have a hall effect position sensor with output ranging from 2.5V-2.9V and is nonlinear w.r.t the measured position. So I want to use a variable gain amplifier that can amplify the raw output to 0-5V and make it as linear as possible.

I imagine in my case I only need a simple differential amplifier with an adjustable gain. However, VGAs like AD605 seems a bit too complex for me to use, because I had some hard time with the output common mode voltage. 

Is there a very basic VGA that takes in DC input and can amplify it with an adjustable gain? Or maybe an evaluation board can also be helpful.

Thank you,

Parents
  • Hello again Hank, 

    One more option for you -- are you set on using a Hall effect sensor? You could also use an AMR sensor for your application. The ADA4571 has an integrated sensor and conditioning circuit and is suitable for position sensing. I highly recommend you check out the reference design which interfaces the ADA4571 with the AD7866. The documentation includes data for linear position measurements and should have everything you need to implement the solution.

    Thanks, 

    Kris

Reply
  • Hello again Hank, 

    One more option for you -- are you set on using a Hall effect sensor? You could also use an AMR sensor for your application. The ADA4571 has an integrated sensor and conditioning circuit and is suitable for position sensing. I highly recommend you check out the reference design which interfaces the ADA4571 with the AD7866. The documentation includes data for linear position measurements and should have everything you need to implement the solution.

    Thanks, 

    Kris

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.