Post Go back to editing

Low Frequency Operation of the Amplifier

Category: Datasheet/Specs
Product Number: AD604

I'm using the AD604 as a low-frequency amplifier from 2 kHz to 2 MHz. Figure 17 only shows input-referred noise from 100 kHz up. Is there characterisation data or a typical 1/f corner for the preamp below 100 kHz? I'd like to know whether the 0.8 nV/√Hz still holds below 10 kHz.

Also: Table 1 lists input bias current as "−27 mA" but Figure 34 shows 27 µA. So, I assume mA is a typo?

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.