Post Go back to editing

ad8334

Category: Hardware
Product Number: AD8334
Hi ,
I have designed a Variable Gain Amplifier (VGA) circuit using the AD8334, bypassing the internal LNA section.
 Instead, I am applying an external differential signal directly to the VGA inputs (VIP1 and VIN1). The output of the AD8334 drives a THS4131 differential amplifier.
Currently, the AD8334 IC is overheating immediately upon power-up.
I have detailed my schematic layout below [or: attached the schematic details]. Could you please review the configuration and share your feedback on what might be causing the overheating?
  • Hi  

    Thank you for your question. Let me check this internally with the team and review the available information. I will get back to you once I have an update.

    Best regards,
    Ian

  • Hi  

    After reviewing the schematic, we recommend checking the following:

    1. The LMD1 - LMD4 pins are left floating. These pins are connected to the LNA bias circuitry and should be bypassed to ground using 0.1uF capacitors, even when the LNA signal path is bypassed.
    2. Output clamp resistors are 100 ohms, which is below the values listed in Table 8 of the datasheet. Please verify the intended output clamp level and select the appropriate resistor values.
    3. Exposed pad must be properly soldered to PCB ground for heat dissipation.

    Could you also share the measured AD8334 supply current during power-up and confirm whether the overheating occurs with no input signal applied?

    Best Regards,
    Ian

  • Hi Ian,


    Thanks for your feedback and recommendations regarding the AD8334.
    I will measure the supply current during power-up and update you with the findings.
    Regarding the LMD pins: We are using a total of 16 AD8334 ICs on a fully assembled PCB. Connecting a 0.1 µF capacitor to each individual LMD pin  would require adding 64 capacitors using jumper wires. Instead of connecting individual capacitors for the four LMD pins on each IC, can I short the four LMD pins of a single IC together and connect them to ground through a single 0.1 µF capacitor?
    Additionally, I will remove the clamp resistor (allowing the default limiting level to revert to 4.5 V p-p), monitor the IC current and heating, and update you tomorrow.

    Thanks and regards,
    Keshav

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.