Post Go back to editing

Reverse Current Protection Not Working

Category: Hardware
Product Number: MAX14523A , MAX1452

I tested the IC by providing 5V to the IN and ON pins. The output is loaded with 400 mA and everything is working.

Then I externally drove the output to 5.2 V. Reverse current is flowing through the IC. It gets desaturated. In my opinion, this should not happen.

Does reverse current protection always work?

Greetings, Andy