Post Go back to editing

Reference design for cascading all 4 channels in an AD8334 amplifier?

Category: Hardware
Product Number: AD8334

Hi,

A ~80dB VGA circuit that we have been using is literally two AD8331 EVAL circuits connected together, and I'm hoping to replace them with a single AD8334 with all 4 channels tied together to achieve similar result with less components.

Is it possible to connect the VOL1/VOH1 to VIN2/VIP2, then VOL2/VOH2 to VIN3/VIP3, VOL3/VOH3 to VIN4/VIP4 respectively, bypassing LNA2, 3, 4?

Is there a reference design out there that we could use? 

Thank you!

  • Hi  

    Yes, you can cascade the channels of AD8334. However, please note that AD8334 does not provide independent gain control for each channel. Instead, Channels 1 and 2 share GAIN12, and Channels 3 and 4 share GAIN34, so gain must be planned carefully. You may also want to consider bandwidth and noise accumulation to ensure stability and linearity.

    Regarding a dedicated reference design, we do not have one for cascading all four channels. That said, we do have AD8334-EVALZ available for prototyping and validation which may serve as starting point for evaluating cascaded configurations.

    Best Regards,
    Ian

  • Hi, can the LNA pins (INH, LOP, LON, LMD) be left floating (NC) if the LNA is unused? Do we need to follow any specific layout or termination rules when operating only the VGA?"

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.