| SLA Status | Assignee | Support Status |
|---|---|---|
| SLA Closed. Met after 54 hours |
maaarmas MStokowski |
Awaiting Company Response |
AD8337
Production
The AD8337 is a low noise, single-ended, linear-in-dB, general-purpose variable gain amplifier (VGA) usable at frequencies from dc to 100 MHz; the −3...
Datasheet
AD8337 on Analog.com
LTspice
Production
LTspice® is a powerful, fast, and free SPICE simulator software, schematic capture and waveform viewer with enhancements and models for improving the simulation...
LTspice on Analog.com
I'm planning on using the AD8337 VGA for a new design. When simulating the part, however, I noticed unexpectedly high output offset voltage present, seeming to disagree with quoted datasheet specifications.
The output offset voltage seems to be 50mV higher than expected, but the characteristic shape of the offset across gain setting seems to match.
I'm using Revision D of the SPICE model released in 2019 (the model currently posted on the website).
I've attached screenshots of my LTSPICE circuit and screenshots from the datasheet I'm referencing (pg. 22 of AD8337 datasheet). Notice the difference in output offset voltage between the simulation and the datasheet screenshot.


It seems like the SPICE model for this IC has historically had a lot of issues (though these seem to typically involve single-supply operation), see:
- AD8337 / SPICE MODEL Dynamic Range
- Simulation not working for certain values on the Vgain pin
- How can I correctly connect the AD8337 spice model?
Please ensure the SPICE actually represents true device performance. Incorrect SPICE models make me hesitate to buy ADI products.
Hello govish87,
Currently, we are on a holiday break and we kindly request for your patience and understanding. We'll verify the offset voltage issue on dual supplies once we get back at the office.
Apologies for the inconvenience caused. I also agree that the spice model has an issue with single supply operation as I've already reported this internally in the past.
Best regards,
Paul
Hello govish87,
Currently, we are on a holiday break and we kindly request for your patience and understanding. We'll verify the offset voltage issue on dual supplies once we get back at the office.
Apologies for the inconvenience caused. I also agree that the spice model has an issue with single supply operation as I've already reported this internally in the past.
Best regards,
Paul
Hello govish87,
I've also used the SPICE web model of AD8337 and was able to get a result quite similar to Figure 74. (Vout = 4mVpp)

Please take note that on Figure 74, Vs = +/-2.5V was used. In addition, the ramp signal applied on the Vgain pin has a frequency of 1kHz. This could be the reason why you have obtained a different result from what is shown on Figure 74.
I hope this helps.
Best regards,
Paul
Hi Paul,
Thanks for your response, and hope you had a good holiday season.
I'm still slightly confused, however. Here's an excerpt from the electrical characteristics section of the datasheet--note the Output Offset Voltage specified at +/- 25mV worst case at peak gain (though I understand that this measurement is also made with +/-2.5V supplies):
Does output offset performance change significantly across supply voltage variance?
<EDIT>: To answer this question, I see this chart in the datasheet:
There does seem to be elevated offset voltage at increased supply, but still seemingly not on the order of the +50mV that I've been observing </EDIT>
Regardless, I associate Output Offset Voltage to be a DC characteristic in any case--why is it fair to measure output offset with an AC waveform? Is there a particular part of the SPICE model that may be responsible for this discrepancy between DC and AC offset performance, and is that representative of true device behavior?
Best,
Ishaan
Hello govish87,
- Yes, you are correct. Increasing the supply voltage will also increase the offset voltage.
- As checked also, it looks like the offset voltage of AD8337's SPICE model at +/-5V Supplies were not modeled. Apologies for the inconvenience. In real life, the typical offset voltage performance of the part at +/-5V should look like the one on Figure 15.
Regardless, I associate Output Offset Voltage to be a DC characteristic in any case--why is it fair to measure output offset with an AC waveform? Is there a particular part of the SPICE model that may be responsible for this discrepancy between DC and AC offset performance, and is that representative of true device behavior?
- Please correct me if I'm wrong. Are you referring to the offset voltage plots of Figure 15 and Figure 74? Please take note that the voltage at the VGAIN pin continuously changes, which effectively changes the gain and thus, the output offset voltage. The offset voltage specification from the electrical characteristics table were only taken at a specific gain setting (VGAIN = 0.7V, 24dB). The output offset voltage spec is a DC spec.
Ex: Looking at the table below, the acceptable output offset voltage value for linear operation is from -25mV to +25mV, (+/-5mV, typically) when Vs = +/-2.5V
|
Now, if we take a look again at Figure 74, at around Vgain = 0.7V, we can get an offset voltage value of approximately -1.5mV. This value directly correlates with the Output Offset Voltage spec from the table above. -1.5mV is within the accepted output offset voltage value specified.
Best regards,
Paul
Hi Paul,
Thanks for the reply again. I'm curious about why I'm seeing different behavior of the output offset voltage in my DC operating point simulation than what you're seeing in the transient simulation--is there a characteristic of the AD8337 that leads to this discrepancy? I would expect a characteristic curve like the one shown in Figure 15, rather than the one I'm seeing in my LTSPICE charts.
My hypothesis is that this is likely because operation at +/-5V split supply is not captured. Would it be possible to get a corrected SPICE model in the near future with device characteristics more completely modeled? I think this would help folks with issues similar to mine + the ones highlighted in the original post.
EDIT:
I quickly verified, and with +/-2.5V supplies, the results for the DC operating point simulation are as expected; see below:
The final answer to my original question is *because operation of the AD8337 with +/-5V supplies is not accurately modeled*. It would still be desirable to get a corrected SPICE model in the near future with device characteristics more completely modeled. I think this would help folks with issues similar to mine + the ones highlighted in the original post.
Best,
Ishaan
Hello govish87
Apologies for the inconvenience. As I mentioned on my last reply, the offset voltage of AD8337's SPICE Web model at +/-5V Supplies were not modeled. I'll report this internally for it to get fixed.
But rest assured that in real life, the typical offset voltage performance of the part at +/-5V should look like the one on Figure 15.
Regards,
Paul
Sounds good!
Thanks for all the insight and support--I really appreciate it.
-Ishaan