AD8338
Recommended for New Designs
The AD8338 is a variable gain amplifier (VGA) for applications
that require a fully differential signal path, low power, low noise,
and a well-defined...
Datasheet
AD8338 on Analog.com
This is regarding AD8338 I am using in VGA mode. The gain voltage set to 0.8 Volt. I am giving single input and taking single output. Deto pin Grounded. 0.1uF Capacitor connected between VREF and OFSN pins. 4.7V Power supply is given to the circuit.
200KHz, -40dBm signal is given as input.
With this configuration, I am not getting gain, no output.
Only I starts getting output when I slowly downs the gain voltage level from 0.8V to 0.6V. But, at this stage I am not getting my desired gain which is 60.
Pics and schematic is attached, What should be the change required to get desired gain of 60 with working output. My input range is 10Khz - 300KHz.