Post Go back to editing

AD8338 VGA Mode, no output

Thread Summary

The user is experiencing no gain and no output with the AD8338 VGA in a single-ended configuration at 200 kHz, -40 dBm input. The final answer suggests grounding the DETO pin, connecting VAGC to VREF, removing C140, replacing R90 with a higher resistance (1 MΩ or higher), and directly measuring the output after C146. The user emphasized the urgency due to delivery delays and the critical nature of the VGA in the receiver IF path.
AI Generated Content
Category: Hardware
Product Number: VGA

This is regarding AD8338 I am using in VGA mode. The gain voltage set to 0.8 Volt. I am giving single input and taking single output. Deto pin Grounded. 0.1uF Capacitor connected between VREF and OFSN pins. 4.7V Power supply is given to the circuit.

200KHz, -40dBm signal is given as input.

With this configuration, I am not getting gain, no output.

Only I starts getting output when I slowly downs the gain voltage level from 0.8V to 0.6V. But, at this stage I am not getting my desired gain which is 60.

Pics and schematic is attached, What should be the change required to get desired gain of 60 with working output. My input range is 10Khz - 300KHz.

Parents Reply Children
  • Hello  and ,

    Apologies for the delayed response. I was out of office for a few days and just got back today.

    I quickly looked on your schematic, and I would like you to implement these changes:
    - When the AGC function is not used, the DETO pin needs to be connected to GND and the VAGC pin needs to be connected to pin VREF only. I would like to recommend removing C140 on the schematic.
    - Since you are not using OUTM's Output, please replace R90 with a higher resistance value. (Ex. 1Meg or higher) 51ohms is too little and could cause high output current draw and high power dissipation that could raise the junction temperature above the safe levels, potentially damaging the part.
    - Remove L19 and C147 and directly measure the output after C146.


    Let me know the test results once you've got them.

    Best regards,
    Paul

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.