Post Go back to editing

AD8330 LTspice simulation error

Thread Summary

The user is experiencing simulation errors with an AGC circuit using the AD8330 DC servo loop, specifically 'Node U1:N662042 is floating and connected to current source G:U1:_G2' and 'Time step too small; initial timepoint: trouble with node n007'. The support engineer suggests connecting the OFST pin to GND as a workaround, which has previously yielded results despite the errors. The AD8330 model is known to have issues, and a fix is pending.
AI Generated Content
Category: Hardware
Product Number: AD8330

I am trying to build an AGC circuit with DC servo loop to keep my output AC signal around 0V. While simulating I get two errors

1- "Node U1:N662042 is floating and connected to current source G:U1:_G2" 

2- Fatal Error: Analysis: Time step too small; initial timepoint: trouble with node "n007"

I downloaded the symbol of AD8330 from Analog devices website and changed the pins according to the datasheet. 

Signal generation AGC DC servo.asc

Parents Reply Children
No Data