Post Go back to editing

AD8330 LTspice simulation error

Thread Summary

The user is experiencing simulation errors with an AGC circuit using the AD8330 DC servo loop, specifically 'Node U1:N662042 is floating and connected to current source G:U1:_G2' and 'Time step too small; initial timepoint: trouble with node n007'. The support engineer suggests connecting the OFST pin to GND as a workaround, which has previously yielded results despite the errors. The AD8330 model is known to have issues, and a fix is pending.
AI Generated Content
Category: Hardware
Product Number: AD8330

I am trying to build an AGC circuit with DC servo loop to keep my output AC signal around 0V. While simulating I get two errors

1- "Node U1:N662042 is floating and connected to current source G:U1:_G2" 

2- Fatal Error: Analysis: Time step too small; initial timepoint: trouble with node "n007"

I downloaded the symbol of AD8330 from Analog devices website and changed the pins according to the datasheet. 

Signal generation AGC DC servo.asc

Parents Reply
  • Hello ,

    I agree with , the spice model of AD8330 has a problem and I already submitted an internal request in the past for it to be fixed. Currently, it is still on queue for a fix.

    For the meantime, can you try connecting the OFST pin to GND and observe if you will get some results even when there is an error? In the past, I was able to get some results even when there is an error when I tried connecting the OFST pin to GND:


    But when I make the OFST pin floating or connected a capacitor to it, I wasn't able to get any results aside from the error.

    Regards,
    Paul

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.