Post Go back to editing

Simulation not working for certain values on the Vgain pin

Thread Summary

The user encountered issues simulating the AD8337's frequency response/bode plot, where the circuit acted as a strong attenuator for Vgain ≥ 0V. The final answer confirmed a problem with the SPICE model when using a single 5V supply and a reference equal to half the supply voltage. The workaround is to use dual supplies with GND as the reference. An accompanying answer noted that the single 5V supply solution has not been resolved.
AI Generated Content
Category: Software
Product Number: AD8337
Software Version: LTSpice v24.1.0

I'm considering using the AD8337 in the design and would like to simulate the frequency response/bode plot.  However when I set the Vgain to 0V or greater the simulations results show it acting as a big attenuator.  For example when Vgain = -0.2V the circuit has around 8 dB of gain as expected.  But when I test for Vgain = 0V or higher which is suppose to give higher gain than the circuit simulations fails and it has more than 200 dB of attenuation.

Thanks,


Sojhal

Parents
  • Hello ,

    In addition to your circuit above, I've connected a 2.5V source to the VCOM pin as instructed on the data sheet to make sure that we are not missing something important when operating the part in single supply. But it looks like the SPICE model of AD8337 has a problem when being operated at a single supply and with a reference equal to half the +Vs. 
      

    I'll submit a request to get the SPICE model fixed. For the meantime, you can try operating the SPICE model in dual supplies. Currently, the model seems to work with dual supplies and GND as a reference as shown below: 





    Regards,
    Paul

  • Hello, I am interested in the single 5V supply solution but haven't managed to get it working. I assume the LTSpice model has not been fixed yet, is that the case?

Reply Children
No Data