Post Go back to editing

AD8337 / SPICE MODEL Dynamic Range

Category: Datasheet/Specs
Product Number: AD8337

Hi,

I am simulating an AD8337 using the SPICE model provided. With pre-amp Gain x2 (6dB) and VGain -600mV (0dB). With power supplies of the part set at +-2.7V, the output is 'compressed' and saturated for input levels higher than about +-630mV. VCom is set to GND. This doesn't seem to make sense based on datasheet values, since the output dynamic range should be at least Vcom+-1.3V.

Am I missing something or is it a simulation model artifact?

Thank you for your help. 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.