AD8336
Production
The AD8336 is a low noise, single-ended, linear in dB, general-purpose variable gain amplifier, usable over a large range of supply voltages. It features...
Datasheet
AD8336 on Analog.com
Hi nalluri ,
It seems that there's an issue with your posted problem since it is only a gray color. Can you post your question again or reply to this thread your question?
Thank you!
Regards,
Mae
Is there any possibility to limit the frequency above 20MHz signal in the above design.in the above design we are setting Vgain as 0 and 16db gain we are expecting in our circuit. the gain is coming .but for higher amplitude values i,e above 80mVpp1-20Mhz is ok but 30-40Mhz freq range the signal is not proper .can you help what is the reason behind it.?
Hi,
In AD8336 preamplifier output some offset is there.after it is giving to VGA also it is not removing that offset .finally my IC output is coming with offset is it expected behaviour of AD8336.
if it seems to be expected then how can i remove that offset it is effecting the total my TX path.
with increase of frequency from 1-40 MHz VGA output is increasing what is the reason .if that is also expected where these are mentioned datasheets .Clarify?
Reply as soon as possible.
it is one of my VGA output voltage.why it is not properly biased?