Post Go back to editing

AD8331 mixed frequency components

Category: Hardware
Product Number: AD8331

Hi, 

I'm Evaluating the AD8331 on the evaluation board AD8331-EVALZ. However I observed mixing products like below photos:

Setting: LNA and VGA actived, 5V power supply provided by LDO ADP7104, Hi-Gain Mode, Slope=UP, Rclapm=open, Vctrl=0.51 (external power supply), Pin=-14dBm 

@10MHz

@20MHz

@30MHz

Where do these sideband spurious come from ? They have the same freq. offset about 4-5MHz to the fundamental. From measured P1dBin at this setting the AD8331 is not saturated. Need urgent help, please...

Thanks in advances,

XL 

Parents
  • Hi,

    It seems that your signal amplitude is slightly modulated by a 4.6MHz signal. This can enter at the gain control pin, so check that signal. Also, check some other points of the system if you see any parasitic voltage with this frequency (maybe on the input or output of the ADP7104, or on some of the grounds of the connected devices). Are you sure that the input signal is free from this?

Reply
  • Hi,

    It seems that your signal amplitude is slightly modulated by a 4.6MHz signal. This can enter at the gain control pin, so check that signal. Also, check some other points of the system if you see any parasitic voltage with this frequency (maybe on the input or output of the ADP7104, or on some of the grounds of the connected devices). Are you sure that the input signal is free from this?

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.