Post Go back to editing

AD604 amplifier

Category: Hardware
Product Number: AD604

Hi 

I am using AD604 in my project, i am not sure how this is working,

G (20 dB/V) = 20 × VGN – 5, VREF = 2.500 V

Vref input is 2.5V, VGN is 0.5volt with this input, 

I am not getting gain as per the above formula, instead i am getting 0db gain for the first channel instead of 15db gain.

It is having R-1.5R ladder network with 7 tap, Using preamplifier gain as 14db by connecting FB pin to Output pin of preamplifier 1 stage and fixed 34.4db of gain at the output, this itself gives 48.4db of gain, what is the use of ladder network attenuator gain of 48db.

please let us know how it works and what is the use of using this amplifier in the RF front end.

Thanks 

Edit Notes

Updated post to new ask a question form
[edited by: GenevaCooper at 11:51 AM (GMT -4) on 25 Sep 2022]