Does this IC supports unidirectional current sensing if I connect VREF pins to ground?
MAX49925
Recommended for New Designs
The MAX49925 is a bidirectional current-sense amplifier (CSA) with an input common-mode range that extends from -40V to +76V, making it suitable for 48V...
Datasheet
MAX49925 on Analog.com
Does this IC supports unidirectional current sensing if I connect VREF pins to ground?
Hi Arikayaaa,
Yes, you can use MAX49925 for unidirectional current sensing. Here's a sample simulation with Vref pins connected to ground for gain of 10:
Best regards,
Ian
Hi Arikayaaa,
Yes, you can use MAX49925 for unidirectional current sensing. Here's a sample simulation with Vref pins connected to ground for gain of 10:
Best regards,
Ian