Post Go back to editing

MAX16913A Short-Circuit Detection Current and RSENSE Selection

Category: Hardware
Product Number: MAX16913A , MAX16913

Dear EngineerZone,

Currently using the MAX16913A, and we have several questions regarding the short-circuit detection current and RSENSE selection.

Based on the datasheet, when RSENSE = 0.65 Ω, the short-circuit detection current can be calculated as:

  • ISC = 100 mV / RSENSE = 153.8 mA

In theory, when the load current exceeds the ISC threshold (approximately 153.4 mA), the output (VOUT) should be shut down.

However, we would like to clarify the following points.

Q1. Short-Circuit Current Specification (340 mA)

In the Features section, a current value of 340 mA is mentioned.

  • Is this value based on 2 × ISC,

  • or is it related to the Absolute Maximum Ratings (ISENSE / IOUT = 340 mA),

  • or is there another interpretation or operating condition that explains this value?

Could you please clarify the meaning and usage condition of the 340 mA specification?

Q2. RSENSE Value Below 0.65 Ω

The datasheet specifies the minimum RSENSE value as 0.65 Ω.

Could you please confirm whether using RSENSE = 0.5 Ω / 0.55 Ω / 0.6 Ω is acceptable in practice? If not recommended, we would appreciate clarification on the specific limitations or risks.

Q3. Higher Short-Circuit Detection Current Requirement

The customer plans to use a normal load current of approximately 180 mA. Is there an alternative device or a similar ADI solution that allows the short-circuit detection current to be set above 220 mA?

Thank you very much for your support.

Parents Reply Children