Hi all,
I am testing a circuit like this. The IC1 in my case is the MAX4210D and Rsense=1R,Rlimit1=0,Rlimit2=1000R,R1=11k and R2=680R. V+ is 10V and Vcc 5V

I have tested two opamp: opamp 1 phase margin 50° and opamp2 phase margin 80°.
With opamp2 the circuit works quite well ( only few ringing)

While with opamp1 the circuit oscillates

Oscillation occurs at around 50kHz

Since my goal is to use opamp 1 given other opamp specs, can you suggest how to stabilize the circuit? Vset change very slowly so I am not interested in reaching high bandwidth
i tried to insert a capacitor here but the oscillation only goes to lower frequency

I hope you can help