Post Go back to editing

MAX4210 constant power source oscillates

Category: Hardware
Product Number: MAX4210

Hi all,

I am testing a circuit like this. The IC1 in my case is the MAX4210D and Rsense=1R,Rlimit1=0,Rlimit2=1000R,R1=11k and R2=680R. V+ is 10V and Vcc 5V

I have tested two opamp: opamp 1 phase margin 50° and opamp2 phase margin 80°.

With opamp2 the circuit works quite well ( only few ringing)

While with opamp1 the circuit oscillates

Oscillation occurs at around 50kHz

Since my goal is to use opamp 1 given other opamp specs, can you suggest how to stabilize the circuit? Vset change very slowly so I am not interested in reaching high bandwidth

i tried to insert a capacitor here but the oscillation only goes to lower frequency 

I hope you can help

  • Hello Topspin, 

    if you want to compensate your feedback loop of the opamp, it is not sufficient to add capacitive feedback. Cause the feedback capacitor goes directly to the low impedant output of the MAX4210. The output driver at pin 8 of the MAX4210 competes directly with the capacitive feedback of your opamp. The compensation may work, if you add not only the capacitor, but also a resistor as shown below. 

    I think your oscillation frequency is ~100kHz? Then you may try an RC-combination in the range of R·C≈1µs to get some additional phase margin for your opamp. 

    best regards

    Achim