Greetings,
If using the AD8479 to monitor cell voltage, does the reference of the IC need to be connected to the battery return line? I have a battery with 24 cells in series. I plan to use a differential voltage monitor on every cell. If the ground of the sensing circuit is completely isolated from the battery circuit, will the AD8479 still accurately measure the differential voltage of the individual cells?