Post Go back to editing

Pin Spacing

Category: Hardware
Product Number: LTC6091

Hello,

I'm slightly confused by the pin spacing on LTC6091. The amplifier is rated for +-140V and rail-to-rail but (I think, please correct me if wrong) if I apply 140V to one of the supply pins (say V+A) and want GND at the OUTA then there's 140V separated by a clearance of 0.5mm. From what I can tell IPC-2221B states the clearance should be a minimum of 0.6mm.

Could you please offer advice on how to proceed with this.

Thank you

Thread Notes

Parents Reply Children
  • Hi Gilbeys,

    Thank you for your reply.

    Does the IPC-2221B standard not apply to the pins as well? They are within 0.5mm of each other, less than the 0.6mm. I also could not have a trace 0.6mm apart from each other if they have to each go to the pins which are 0.5mm apart.

    I look forward to your response, thank you

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.