Post Go back to editing

some questions about EVKIT datasheet

Thread Summary

The user encountered issues with their APD circuit using the MAX40660, noting discrepancies in the current calculations from Table 2 of the MAX40660 Evaluation Kit. The final answer clarifies that Equation 1 is only valid for small signal currents below 100uA, not for the mA-range currents listed in Table 2. The user is still awaiting further clarification on the specific values.
AI Generated Content
Category: Datasheet/Specs
Product Number: MAX40660

Hi, I used a MAX40660 to make a APD circuit,but it doesn't work.So I read the MAX40660 Evaluation Kit to compare my circuit with it. In my opinions,the Kit use an input Voltage to simulate optical current.When I read "Current Pulse Measurements", I noticed that the data of Table 2 made me confused,if  INPUT SERIES RESISTANCE RS = 1,  GENERATOR INPUT HIGH VOLTAGE = 0.855V,  GENERATOR INPUT LOW VOLTAGE =0.15V, according to the Equation 1, the current is not 10 mA.I want to know where I went wrong. My understanding is that the VCAL-SET here is the voltage I input.Thank you.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.