Post Go back to editing

About Input offset voltage

Category: Datasheet/Specs
Product Number: LT6105

Hello team,

I understand that when using the LT6105I and the -IN voltage is within
the range of 0V < V(-IN) < 1.6V, the input offset voltage falls within
the red-framed range in the table below.

Could you please confirm if my understanding is correct?

Best regards,
Tsuyoshi Tokumoto

  • Hi Toku,

    Good day. The -IN voltage should be within the input voltage range, Vs+,Vs- which is within -0.3 to 44 V. It is not affected by the input offset voltage. Can you clarify where did you get the -IN voltage range? Thank you.

    Regards,
    Gilbeys

  • Hi Gilbeys-san,

    Thank you very much for your prompt reply.
     
     Based on the following information in the datasheet,
      I understood that the input offset voltage may vary depending on
     the -IN voltage range:

     ①The graph on page 6 of the datasheet.

     ②The description in the “THEORY OF OPERATION” section on page 12.
     ③The explanation in “The Two Input Stages Crossover Region” on page 14.

     Is my understanding incorrect?

    Best regards,
    Tsuyoshi Tokumoto

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.