Post Go back to editing

Internal resistor precision

Category: Datasheet/Specs
Product Number: AD8210

Dear Support,


According to the AD8210 datasheet, the internal series resistors on the IN+ and IN- inputs are 2kohm.

Can you tell me what the tolerance of each of these is?

I would like to calculate how much inaccuracy it causes if the external series resistor is >10ohm.

Best regards,

  • Hi  ,

    Good day. Unfortunately, there were no specifications for the tolerance of the internal resistors. However, the internal resistors' effect on the gain is already measured and specified based on the gain accuracy of the part. Here is the specification for 5 V:

    You can use this value for the error calculation of your system. Thank you.

    Regards,
    Gilbeys

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.